AXIS#.PL.KP

Description

AXIS#.PL.KP sets the proportional gain of the position regulator PID loop.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Hz

Range

0 to 500

Default Value

3.27

Data Type

Float

See Also

AXIS#.PL.KI

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.PL.KP

500ch

04h

Unsigned32

-

1000:1

Read/Write

No

AXIS2.PL.KP

510ch

04h

Unsigned32

-

1000:1

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.PL.KP

5908

1714

Signed32

Read/Write

-

AXIS2.PL.KP

71444

1171

Signed32

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.PL.KP

5908

Float

Read/Write

-